DOUT#.SOURCEID

Description

DOUT#.SOURCEID sets the digital output source ID, for sources that require an ID.

Examples

Usage

DOUT#.SOURCEID can be used to select the compare channel when DOUT#.SOURCE = 4 (Compare).

Code

These commands set the source of digital output 2 to compare channel 1, and digital output 3 to compare channel 2.

--> DOUT2.SOURCE 4
--> DOUT2.SOURCEID 1
--> DOUT3.SOURCE 4
--> DOUT3.SOURCEID 2

Context

See Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000  
Added Compare channel support 02-06-00-000  

General Information

Type Read/Write
Units N/A
Range 1 to 2
Default Value 0
Data Type Integer
See Also N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

DOUT1.SOURCEID

360ah

02h

Unsigned8

-

-

Read/Write

No

DOUT2.SOURCEID

360bh

02h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

21200

1

21200 (0x52d0)

DOUT1.SOURCEID

Unsigned8

Read/Write

Yes

21201

1

21201 (0x52d1)

DOUT2.SOURCEID

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

DOUT1.SOURCEID

21200

Unsigned8

Read/Write

-

DOUT2.SOURCEID

21201

Unsigned8

Read/Write

-